Tool/software:
I am using BQ25628 to charge a battery and also provide power to the rest of the system. sometimes the system voltage (SYS) drops to ~2.8V and it causes the LDO after this to go down. the battery voltage is stable at all times. the ILIM resistor is set to provide ~560mA while the system does not take this much current, and the battery output current is less than this. the BQ25628 log is attached. before system voltage go down, I see watchdog is getting enabled while we keep it disable all the time. as I know, watchdog does not cause the system voltage to go down and just brings the settings back to POR moment. QON pin is not connected to anything, and it should be high with an internal 250K pullup which I confirmed this pin is high during voltage drop.
the I2C BUS is shared between this chip and a fuel gauge. does any sort of communication to the fuel gauge or anything on this BUS can cause this problem?
Please advise.
Thank you.