This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2936: Large reel equivalent for the LM2936Z-5.0/NOPB?

Part Number: LM2936


Tool/software:

Hi all,

do we have an equivalent large reel for the LM2936Z-5.0/NOPB?

Is the LM2936Z-5.0/LFT4 a good fit? I'm interested to understand the differences with the suffix LFT4 and NOPB.

Thanks,

Adrian

  • Hey Adrian,

    It looks like the LM2936Z-5.0/NOPB is in a 1800 reel size with no 2000 or 2500 option. The NOPB refers to no lead, where the LFT do not specify that lead is not used. Do you have Iout, Vin, Vout requirements? There is likely a better solution here. The TO-92 is a legacy package with lots of modern alternatives that I would recommend. 

    Thanks, 

    McKyla

  • McKyla,

    so you do confirm the LM2936Z-5.0/NOPB comes in a reel carrier? Somehow Arrow mentioned it comes in bulk.

    The size of the reel is not a problem, as long as it comes in a a reel.

    Customer is not evaluating to change device now, just looking for the large reel of the device being used.

    BR,

    Adrian

  • Hey Adrian, 

    Apologies for the delay here. I cannot speak for Arrow, but our LM2936Z-5.0/NOPB indicated that this comes in a small tape and reel. 

    Thanks, 

    McKyla