This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24715: What is the function of the minimum system voltage setting?

Part Number: BQ24715

Tool/software:

dears,

what is the function of the minimum system voltage setting? my understanding is that it is used to prevent the system voltage to drop to a very low voltage when battery is depleted. but will it limit the battery to discharge below the minimum system voltage we set? I think it should not limit the battery discharging,  the battery may discharge till the system or battery protection function to disable the discharging. am i right? 

thanks a lot!