This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21540: Risk for immersion cooling analyzement

Part Number: UCC21540

Tool/software:

Hello experts, 

I am Erick, sales in Taiwan, I would like to kindly request for your help with analyze or give me any feedback if there could be any risk to put UCC21540 in immersion cooling.

The immersion cooling process is soaking the server in a non-conductive liquid, conducting heat through direct contact with the hot part and the flow of the liquid, eliminates the need for dissipating the heat part.

The below information may help you to analyze the impact putting device in  the selective immersion cooling.

  1. Immersion cooling process, 
    https://2crsi.com/immersion-cooling
  2. The solution our customer use is Noah 3000, which is consist of 100% Perfluorononene epoxides
  • Hi Erick,

    In terms of the material compatibility of UCC21540 with the immersion cooling solution you highlighted above, please refer to this website, which allows you to look up the material contents for any of TI's parts. Utilize this information to make a conclusion about whether it will work with your solution. Generally, TI uses standard encapsulations for most of our parts, so abnormal behaviors will likely not arise regarding the part's interaction with the chemicals in the cooling compound.

    Finally, please refer to the insulation specifications for UCC21540 on page 7 in the datasheet. Almost all of these specifications are measured in air, but there are some measured in dielectrics.

    Best regards,

    Will

  • Hello Will, 

    OK, really thanks for your help