This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74704-Q1: Simple 24V load dump protection

Part Number: LM74704-Q1
Other Parts Discussed in Thread: LM74800-Q1

Tool/software:

Hi,

I am looking for a solution to protect my circuit from a load dump (ISO 16750-2 4.6.4 Test B) in a 24V system. It should either limit/clamp the voltage to max 48V (when clamping it should be able to withstand jump start for 60s) or open the circuit. I went through some of the ideal diodes, but I haven't found the perfect match yet. Reverse polarity protection would be a benefit, but I am not looking for more features - simplicity has priority. Which of your products would you recommend? Thanks