This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5160A: LM5160ADNT || Heat Issue || 48V TO 24V || 2A LOAD

Part Number: LM5160A


Tool/software:

Hi 

We are using LM5160A in our design. 

Below is our design requirement which we done in Design.

Vinput = 48V

V(OUTPUT)= 24V

I(LOAD) = 2A

Below are issue we are facing in our PCB:-

1.  We are getting 18V instead of 24V.

2. After removing R9(130mohm) and Adding zero Ohm resistor in R9. We are getting proper 24V. But we are getting some heating issues. below are mentioned:-

a) with load current = 1A, LM5160A & Inductor(120uH) getting heated.

b) With Load current = 2A, LM5160A & Inductor(120uH). its get repaid heated & output voltage  are varing(10-24V).

After done some change from switching frequency side . We are getting same issue.

1. bydefault 192khz (Ron= 1.24M)

2. 292khz (Ron= 480K)

Inductor part no :-  MSS1210-124KEB