Other Parts Discussed in Thread: TPS35
Tool/software:
Dear all:
our original watch dog IC is S-19400G28A-K8T2U4 ABLIC, we will change it to new Alternative part is TPS35-Q1 serial , full MPN:TPS35CA**LAEDDFRQ1(** is unknow)
In order to get closer to the original design parameters , we select TPS35CA**LAEDDFRQ1.
but there are some question such as:
1. according to TPS35-Q1 spec we choose the MPN TPS35CA**LAEDDFRQ1 as below: see red color
Threshold Voltage is need 2.8v ,this type is it provided? , I can't confirm if 2.8V is available by naming nomenclature show as below

2.Consider our original design and requirements, the PINOUT C is only options,but has some question as below

2-1:we must add new 3 ports is SET0,SET1,/MR from original(ABLIC S-19400G28A-K8T2U4) for new design, cause to new Circuit must be redesigned
if SET0,SET1 has no use anymore ,then it will be set to scaling=1 , like bit[0,0] , How to deal with these 2 ports?Tie to GND, or anything to note ?
if pull it up ,how to do with , such as pull up Resistance Value is ?
2-2:WDI trigger is change to falling edge trigger from rising edge before ,what does software to pay attention for?
2-3:the t_SD timming is no need , it is ok?:marked with red line show :

and what dose this t SD time delay function and it is must necessary?
our original design of ABLIC S-19400G28A-K8T2U4 IC is no equipped with it
our original design of circuits detail is:
the VDD=3.3V
MCU:RH850(Renesas)
TWD=11S
TD=65.2ms
WEN is need
AEC-Q is need

thank you and best regards