Tool/software:
Hello,
we would like to provide constant current to a RGB LED where the 3 LEDs are supplied using a common anode.
Is it possible to use 3x TPS92200 ICs for this purpose?
Best regards and thanks in advance
Andreas
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
we would like to provide constant current to a RGB LED where the 3 LEDs are supplied using a common anode.
Is it possible to use 3x TPS92200 ICs for this purpose?
Best regards and thanks in advance
Andreas
Hi Andreas,
You are right. TPS92200 is not a suitable choice if you need separately controlled 3 RBG LEDs with common anode connection.
Could you please share your end-equipment application, the current range of each LED and the brightness control methods you prefer? I could recommend most suitable device(s) to you.
Thank you!
Best,
John.
Hello John,
thanks a lot for your quick reply, even on a weekend - much appreciated!
We would like to control different kinds of LEDs, mainly TW (2x IC), RGB (3x IC) and RGBW (4x IC), with common anode connection each.
Current per LED channel is only 350 mA or 500 mA. Hence the reason we were first looking at the TPS92200 variant as the TPS92205x series with > 2 A max. current seems oversized for our application.
The brightness control method from the MCU towards the driver IC should be digital (PWM). The control method from the IC towards the LED could be digital (PWM), analog or a combination of both.
Best regards and thanks again for your support
Andreas
Hi Andreas,
Thank you for your reply!
Could you please also provide the input voltage range of each channel? And does it has a requirement about efficiency?
And could you please leave your email, so I could loop application engineers covering other potential devices and marketing guys? We can help you pick the right device based on your application details and project schedule.
Thank you!
Best,
John.
Hello John,
sure, voltage range of the LED types mentioned above is 18-24 V. If for the future use of other LED types also up to 48 V could be supported that would be great, but not a hard requirement.
You can send an e-mail to:
info@ab-smarthouse.com
Best regards and thanks again
Andreas
Hi Andreas,
I have sent you a email. We could continue our conversation via that. Please check if you have received that.
Thank you!
Best,
John.
Hi Andreas,
Since we are discussing via email, I am going to close this thread.
Thanks!
Best,
John.