Other Parts Discussed in Thread: TIDA-050058, TMUX1219, TPSI3050
Tool/software:
I have some questions in design guide : TIDA-050058
1. the 2 MOSFET will be solid-state relay ?
2. the SEL in TMUX1219 , is come from other like MCU io ?
3. the 5V and GND is the LV secondary side ?
4. in this application , whatever the timing of SEL , the EN @ ILOAD always turn on at zero point of AC ?
5. this application cannot control turn off at zero pont of AC right ? if also want to turn off at zero point of AC , how to do the design?
6. in the LOAD side , no mater for AC L or N TO CONNECT TO sw1/ sw2 point ?
7. what's the requirement for SEL signal ?
Thanks1
Meican.