Other Parts Discussed in Thread: BQSTUDIO
Tool/software:
Hi Ti Experts,
We are using the bq76952 BMS IC in one of our projects in host-controlled-mode for a 13S6P E-bike application (1600Wh).
The application was designed some years ago.
During our customer's test, we sometimes see that the bq measures a lower value for cell 11 and a higher voltage value for cell 12. After a shutdown/Reset it works fine again.
In the following snapshot you can see the cell voltages from Cell1 to Cell 13.

The customer charged the bike in the evening. At the next morning after starting the bike the measurement above was taken.
After a restart the voltage measurements were equal again.
The schematic looks like this:


Could it be a problem that the VC14 to VC16 is shorten together or could this be the issue for our behavior?
Now we know that we should do the wiring like it is written here:
But about 4 years ago I think we did not know.
Thanks for helping us.
Klaus