Other Parts Discussed in Thread: UCC27282, , LMG1205, LMG1210
Tool/software:
Using this eval board, it seems that the thermal pad on UCC27282 chip which is thermally connected to a large GND plane is not enough to dissipate the heat created within the chip. I have to use an external fan to keep the chip cooler. I have damaged the 1st eval board without providing air flow for the chip. This chip is driving 2 MOSFETs IRF510 whose output is connected to a 1:9 transformer, low pass filter, and 50 ohm load. Switching frequency is 7MHz. I use the EN input to pulse the RF with a 40% duty cycle.
Do you think I need to provide better heatsinking to UCC27282 and how?
Thanks