This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV713: TLV71310PQDBVRQ1

Part Number: TLV713

Tool/software:

Hello

I am using TLV71310PQDBVRQ1, to generate 1.0V from 1.8V, when i put a bead between the VIN and 1.8V, the max output current only 130mA, after remove the bead the output current can reach 150mA.

the bead part number is: BLM15AG601SH1D, with bead the VIN pin voltage is a little lower, but still above 1.7V, do u know why the bead affect max current?

thanks

Bruce