This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC5350-Q1: UCC5350MC

Part Number: UCC5350-Q1
Other Parts Discussed in Thread: UCC5350,

Tool/software:

Hi team,

When we use UCC5350MC to drive two parallel IGBTs, how to connect clamp pin of UCC5350? Can we connect clamp to G of  two IGBTs? Thanks!

BR

JIawei

  • Hi Jlawei,

    Due to their slower switching dV/dt, IGBTs do not have as bad of Miller injection problem compared to Si Mosfets.

    It is probably best to connect CLAMP to OUT. If you connect CLAMP to G1 and G2, the gates will be shorted together, and it might lead to greater imbalance in current sharing between the IGBTs, if there is a process variation related Vth mismatch.

    If you do see a Miller spike with this circuit, then it is probably better to attache CLAMP to G1 and G2, since current mismatch is a less significant problem than Miller injection spikes.

    I am going to run some tests to further investigate the best solution to this common question, and I will get back to you with the eventual results.

    Best regards,

    Sean

  • Hi Sean,

    Thanks for your reply. Looking forward to your test results.

    For UCC5350-Q1, which one OPN is better for this application scenario? UCC5350MC-Q1 or UCC5350SB-Q1?

    BR

    Jiawei

  • Hi Jiawei,

    The UCC5350M will give you the flexibility to attach CLAMP to G1 and G2 if you discover extra Miller clamping is needed. That is probably the right device.

    Best regards,

    Sean