Tool/software:
Hi,
There is a big package for TPS3422, like SOT23-6 or SC70-6 ?
Thank's.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
There is a big package for TPS3422, like SOT23-6 or SC70-6 ?
Thank's.
Hi Rangel,
We only offer the TPS3422 in the USON (1.45mm x 1.00mm) package. The most similar IC in a larger package (DDF, SOT23 8-pin, 2.9mm x 1.6mm) would be the, TPS3435CAKAGDDFR that can act as a 6.4s push-button with a 200ms reset pulse.
Could you help me understand why you would like to design with a larger package IC? Is this for thermal concerns?
Thanks,
Joshua