The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25149: switching mosfet over heating

Part Number: LM25149
Other Parts Discussed in Thread: CSD17577Q5A,

Tool/software:

Hello,

we have a problem with LM25149 mosfet design - we are using a 24 V input voltage and we are currently outputting 5.3 V. For load we are using 3x parallel resistor with values 1.5 ohms. At the current test setup, we are drawing from the circuit only 2.5 A, and mosfets CSD17577Q5A is heating up to 120 - 130 degrees. If we reduce the input voltage to 14 V we are able to draw 4 A from a circuit and also mosfets reach max 95 degrees.