Part Number: BQ77216
Tool/software:
Hi team,
My customer (Sinoev) would like to use BQ77216, and there are some queations would like to confirm with you.
1. What is the output voltage of COUT and DOUT of the BQ7721611 chip? What is the load capacity? (open-drain output)
2. In addition, from the block diagram of the datasheet, COUT and DOUT are directly connected to VDDD, so I am a little worried about the output voltage of them. Can you help provide the instructions of internal voltage conversion on this? Do you have detailed internal block diagram?
3. In the schematic diagram of the BQ7721611EVM board, it was found that the power supply of VDD is connected to the highest node of the battery through a 100R 0603 resistor. Is the power consumption of this resistor appropriate? Because I need to use COUT and DOUT to drive 2 optocouplers, and the driving current of a single optocoupler needs to be 5mA. In this case, how should the size and package of the resistor between VDD and the highest node of the battery be selected?
Thank you
Ethan