Tool/software:
I have designed a wide-input (12-26V) 5v buck converter using the LM3150. When tested in complete isolation - it works well across my entire input range and keeps a stable 5v at up to 4A as designed. The first part of my system includes an LTC4365 for OV and UV protection. I also added extra gate resistance and capacitance to the FETs of the 4365 in order to reduce in-rush.
The strange thing is that when tested as a whole system, the LM3150 output voltage starts to dip for pretty moderate constant resistance loads (on my e-load)...begins to dip below 5v at ~12ohm. When tested in isolation, there is no dip at all up to my designed current max.
I'm a bit puzzled here - my first thought was that the output of the 4365 is oscillating or not stable, but on the scope it's very stable and corresponds just to the Rds_on losses of the 4365's FETs. I know that the 4365 is the culprit because I am injecting input from the power supply directly at pin 5 of Q101. During these tests, I have no other loads connected and every other part of the board is de-powered.
Ignore that I incorrectly hooked up the LED for the !fault line :)