Part Number: TPS7A26
Tool/software:
hello. In this project, the circuit was constructed using TPS7A26.
I am trying to turn the TPS7A26 Output ON/OFF by controlling the VEN on the FPGA.
When VEN=0, Vout is output as an abnormal voltage instead of 0V. At VEN=0, VFB is 0.2V and 1.73V is output by the feedback voltage.
(@ R1= 7.5M, R2= 1M, VFB =100K) At first, it was designed with R1 = 9.1K, R2 = 1.3K, VFB = 10K (design mistake), Changed to the appropriate R1, R2, and RFB values written in the datasheet.
The circuit diagram is attached below.
Please answer whether the device has been damaged or whether 0V is not output even if VEN=0.