This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2897A: PMP7413

Part Number: UCC2897A

Tool/software:

Dear TI members,
can PMP7413 reference design can be used for

i) voltage input range of 80VDC to 160VDC
ii) Output 5V @ 12A

 is it fine if i modify design to run in the input voltage range from 80VDC to 160VDC 

for output of 5V@12A,

request to please share your views at your earliest convenience for same