Tool/software:
Hi,
I have a couple of quick question on TPS51200.
1. If I don’t want to use the REFOUT pin in my application, can I leave REFIN pin unused? If it is allowed to leave REFIN unused, how should it be connected (pulled down/up via resistor, directly connected to VLDOIN, etc.)?
2. If REFIN is used in the design via VLDOIN and voltage divider (0.6V for DDR4), but REFOUT is not used and just tied to a 0.1uF capacitor to GND, does it have any adverse effects? I know that it should be a problem functionally, but just in case there's anything else that I should be aware of.
Thanks,
Kaitav