Other Parts Discussed in Thread: LM5146-Q1, , LM5145, LM25145, LM5146
Tool/software:
Hi All,
I was planning to use earlier LM5146-Q1 for my DC-DC buck design.
Just came across LV5144 - looks like it is exact pin to pin replacement - except 3 major differences.
Vin max for LV5144 is 95 Volts, Vin max for LM5146-Q1 is 100 Volts.
Ioutmax for LV5144 is 20 A, Ioutmax for LM5146-Q1 is 30 A.
LV5144 is way cheaper than LM5146-Q1.
I have 3 designs - 10 A/20A/30A .
Can you please confirm if I wont be able to use LV5144 for 30 A?
if LV5144 and LM5146-Q1 are 99 percent similar - can LM5144 be used for 30 A also?
Really appreciate your guidance and support.
Thanks
Sahil