This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25731: Can BQ25731 support supercapacitor backup function?

Part Number: BQ25731
Other Parts Discussed in Thread: BQ24800

Tool/software:

Hi Team,

I have a function requirment for supercapacitor Backup(Power input is 12V,Device supply is also 12V,Supercapacitor is 5.5V),I want to know whether  BQ25731 can support below function:

1.When input 12V power is supplied, VSYS supplies power to the device (the voltage is also 12V) and depressurizes the 5.5V supercapacitor

2. In the absence of an input source, supercapacitor supply to VSYS through boost circuit(boost voltage ranges from 7V-12V)

Please help to check whether BQ25731 can support this function,if ok,How to configure the registers ?