This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS536C7: No output on a prototype board using TPS536C7

Part Number: TPS536C7

Tool/software:

I made a prototype board using TPS536C7 and am testing it, but there is no output.(0V)

Could you give me a solution?

The power stage is not a TI product.

〇The voltages on each pin are as follows:

 VCC3.3V、VIN:12V、VREF:1.500V、TSEN:0.797V、PWM:Approx. 1.59V(constant)、ACSP:Approx. 2.5V

〇Error status displayed in FUSION design:

Please let me know if you have any other necessary information.

Best regards.