Tool/software:
Hello and thank you for your support.
We're considering the use of the BQ79616 battery monitor chip within an ASIL-D system and the chip is certified SEooC ASIL-D, while reviewing the safety concept we can see that its safety mechanisms are categorized into three groups:
- Auto: Mechanisms that are passive elements or automatically executed by the ASIC.
- FDTI: Mechanisms or diagnostic functions designed to be handled with external microcontroller assistance within each Fault Tolerant Detection Interval.
- MPFDI: Mechanisms or diagnostic functions designed to be executed with external microcontroller assistance at least once within Multi Point Fault Detection Interval.
I have two questions:
1. Our understanding is that it is not possible to use that chip as a standalone device, and that an ASIL-D rated host controller is required to allow the chip to achieve its rated ASIL, I want to conifrm this and check if there are ways around it, or if there is a way for the controller to have a lower ASIL (B).
2. I would like to understand more the method by which safety mechanisms are assigned these diagnostic groups, for example "SM1: AVDD OV Detection" is designated as FDTI, while "SM2: AVDD UV Detection " is designates as Auto, while both seem to address a somewhat similar concern, it would be helpful to understand how that categorization was decided.
Thank you.