This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS274160: The ESD test problem

Part Number: TPS274160

Tool/software:

Hi E2E,

Our customer is using TPS274160ARLHR to design a product. Some SCHs are as follows:

The problem we encountered was that the voltage of +500V could pass through the ESD surge test; the voltage -500V will burn TPS274160.

We tried to connect two SMAJ28CA in parallel with D20 at the input end of 24V_Field, but TPS274160 would still be burned.

And we have check the ESD Ratings in the datasheet:

In the datasheet, we only see the description of voltage waveform in ESD, but the current waveform is not shown.

We hope that TI can provide relevant explanation and reference.

In addition, the ESD test of -500V failed. What is the reason? Any suggestions for improvement?

Thanks

Best Regards