Tool/software:
Hello TI Team,
regarding to datasheet the TX-Pin should be high impedance in shutdown mode but i am measuring 3,2V at the output.
MCU and BQ75614 have direct connection with each oder and when we turn off the 5V supply (DCDC Converter) of MCU, BQ chip going to shutdown mode because of long communication timeaout (2s).
In this case it starts to flow some current (6mA) from BQ Uart TX-Pin to the MCU over 47R resistance. It seems that current flowing over internal gpio diode of MCU to the 5V-Power.
But TX-Pin shouldnt have any voltage at shutdown mode. Propably because of 6mA current over the TX-Pin and CVDD, is also CVDD volatge is very low (3,51V).
thank you for your help!
sincerely