This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5185-Q1: Vout is dropping at intervals with load and without load.

Part Number: LM5185-Q1
Other Parts Discussed in Thread: LM5185

Tool/software:

Team,

Specs are below :

Vin : 9V - 32V, Vout :15V,  load : 0.5A

Vout is dropping at different intervals without resistor load and with resistor load.

Additionally, with increasing Vin voltage around 32V , transformer primary current is rising more than rated current during that dip interval and saturating but Vout dip slightly gets reduced. 

 What I also noticed from waveforms is Vout is dropping first and then IC is trying to regulate it or something else could be reason ?

Below is the circuit and excel file.

1050.LM5185-DESIGN-CALC.xlsx

Rfb: 73.5K

Rsense : 40mOhms, 

Transformer p/n : 750318114

Below are images without load

With load of 0.4A