This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25750EVM: BQ25750 CV mode charge current swing

Part Number: BQ25750EVM
Other Parts Discussed in Thread: BQ25750

Tool/software:

Hi,

I setted up as below battery and charging voltage & current.

The device works well to change CC mode to CV mode, but it started current swing at close to termination current. (not touch to thermination current)

- Supply voltage : 24V

- Charging voltage 28.99V

- Charging current : ICHG_REG : 4.5A / ITERM : 500mA

- Battery : Li-ion 25.41Vdc(7S2P)

CHG_CVmode_swing.txt
* Created: Fri Aug 30 16:28:21 KST 2024
*
* Format: Register Name  tab Character,\t  Register Address  tab Character,\t  Hexadecimal register value.
* BQZ Container: Charger_1_00-bq25750.bqz
*
Charge Voltage Limit	00	10
Charge Current Limit	02	168
Input Current DPM Limit	06	640
Input Voltage DPM Limit	08	348
Reverse Mode Input Current Limit	0A	640
Reverse Mode System Voltage Limit	0C	3E8
Precharge Current Limit	10	140
Termination Current Limit	12	28
Precharge and Termination Control	14	0F
Timer Control	15	0D
Three-Stage Charge Control	16	00
Charger Control	17	C9
Pin Control	18	C0
Power Path and Reverse Mode Control	19	20
MPPT Control	1A	20
TS Charging Threshold Control	1B	96
TS Charging Region Behavior Control	1C	57
TS Reverse Mode Threshold Control	1D	40
Reverse Undervoltage Control	1E	00
VAC Max Power Point Detected	1F	00
Charger Status 1	21	84
Charger Status 2	22	80
Charger Status 3	23	02
Fault Status	24	00
Charger Flag 1	25	00
Charger Flag 2	26	00
Fault Flag	27	00
Charger Mask 1	28	00
Charger Mask 2	29	00
Fault Mask	2A	00
ADC Control	2B	60
ADC Channel Control	2C	02
IAC ADC - Use Field View	2D	966
IBAT ADC - Use Field View	2F	7C5
VAC ADC	31	2E02
VBAT ADC	33	37E5
VSYS ADC	35	2E8B
TS ADC	37	24E
VFB ADC	39	00
Gate Driver Strength Control	3B	00
Gate Driver Dead Time Control	3C	00
Part Information	3D	02
GM Adjust	61	32
Reverse Mode Battery Discharge Current	62	02

Thanks