Other Parts Discussed in Thread: BQ8050
Tool/software:
Hi TI engineer:
I have two questions about BQ8050 chip substituted, and hope to get a reply
(1)I burned the programs used in the BQ8050 onto the SN8765 chip. Can this program run normally on the SN8765 chip? Are there any hidden dangers? Is there anything I should be aware of
(2)Suppose SN8765 can replace BQ8050.
A pin is a NC pin in the SN8765 manual, but is a defined pin in BQ8050, when SN8765 programme a program that can be used normally in BQ8050, will the NC pin of SN8765 also have the same function as the BQ8050? If the same function cannot be implemented, what is the approximate reason
Looking forward to your reply! thank you!