Other Parts Discussed in Thread: BQ25628, BQ25619, BQ25895M
Tool/software:
Hi
We use VSYS to power the main processor (using a 3.3V LDO). VSYS is stable as long as only the battery is connected, but as soon as power is supplied to VBUS I measure a voltage dip on VSYS which resets the main processor (see image below). No voltage dip can be observed when power is removed from VBUS.
Steps to reproduce:
- Remove VBUS voltage, attach battery, VSYS is stable at 4V
- Main processor boots up and runs stable
- Supply power to VBUS
- VSYS drops to 2V for 12ms then returns to 4V
- Main processor reboots
- Remove VBUS voltage
- VSYS stays stable
It seems like the BQ25629 switches off Q4 after VBUS is supplied. I suspect that the IC needs some time to discover the VBUS type so I tried to set EN_AUTO_INDET to 0 to disable automatic D+/D- detection when VBUS is plugged-in but it does not solve the problem.
Are there any other settings I need to change?
Thanks for your support & best regards
Rashid