Other Parts Discussed in Thread: BQ25713
Tool/software:
Hi,
My name is Antonio López and I have a few questions about the BQ25713B:
- Which is the difference between BQ25713 and BQ25713B?
- Can I make my own PCB with the typical application componentes like in the figure 10-1 from the datasheet or I need more like in the EVM board? (My project is only for charging batteries 1S but I want to configure the charge current).
- And why do you recommend 4- layers instead of 2?(If the recomendation is 4 in which layer are for the power, ground and signals?)
Best regards,
Antonio López