Other Parts Discussed in Thread: BQ51013C,
Tool/software:
Hi all,
I am looking for the next model of this product.
1) Is there a next model of this product?
And will I get sufficient support when I use this device?
The required specifications are as follows.
[Required Specifications]
I would like to charge 1 cell Li-ion battery Qi.
Output 5 W (=4.2 V/1.2 A)
I want to connect directly to the battery.
2) I think we exchange signals at AC1.
I understand that EVM's C14,C15, and C16 are connected to suppress voltage fluctuation at that time.
10uF is recommended, but is there any problem if we add C14,15, and 16 constants to suppress signal change more?
Best Regards,
Ryusuke