Tool/software:
Hi,
If the VIN voltage falls below VDO + VREF, will VOUT be output? Or will the output stop due to an error?
VDO varies depending on the conditions, but for example, if the current VDO is 0.1V and the REF3525 is used, a minimum VIN of 2.6V is required.
In this case,
what happens when VIN = 2.55V or VIN = 2.0V?
My guess is that
when VIN = 2.55V, VOUT is approximately 2.45V.
When VIN = 2.0V, does VOUT output stop?
On the other hand, the customer believes that output stops under both of the above conditions.
Sorry for the basic question, but I would appreciate your answer.
Best regards,
Hiroshi