Other Parts Discussed in Thread: BQ76952
Tool/software:
Hi E2E,
When pairing with the BQ76952, could you please provide the recommended resistance values for the six highlighted FETs?
Thanks!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Tom,
The gate MOSFET resistors could be something like 10-kOhm. For the pull-downs, they should be decently large. But low enough that the gate-source voltage turns-off the MOSFET when it is pulled low.
Now, ensure that the DOUT/COUT pins also connect to CFETOFF/DFETOFF, so that this will properly work.
Best Regards,
Luis Hernandez Salomon
Hello Tom,
I would recommend to not use these pull-down MOSFETs and instead just use the CFETOFF/DFETOFF.
There is no exact values recommended for these resistors. The pull-down could be relatively large to limit current flow through the gate-source zener diode.
Best Regards,
Luis Hernandez Salomon