Tool/software:
Hi,
Could you please share the maximum junction temperature of the IC (HD3SS3220IRNHT)?
Thanks & Regards,
Prabu S
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
Could you please share the maximum junction temperature of the IC (HD3SS3220IRNHT)?
Thanks & Regards,
Prabu S
Hi Prabu,
The max Tj for HD3SS3220 is 115C.
Best,
Shane
Hi Shane,
Thanks for sharing the details.
Could you please clarify the below also?
In datasheet, it is mentioned the current is 0.9mA (max).

Whether this current taken by VCC33 or VDD5 rail?. Also please share the current of each rail?
Thanks & Regards,
Prabu S
Hi Prabu,
VDD5 is the power rail for the CC controller, VCC33 is the power rail for the MUX.
Icc (0.2mA) is the current of VDD5. Iactive - Icc (0.5mA typ) is the current of VCC33.

Best,
Shane