Other Parts Discussed in Thread: BQ24130
Tool/software:
Hi expert,
A question about the charger IC temperature protection. Currently we are working on the charger IC BQ24105. According to the data sheet, there is an equation to calculate the selection of RT1&RT2. But in some cases, for example the RTHcold is 25kΩ & RTHhot is 5kΩ, the result of RT1 would be -370kΩ but negative value is not applicable. I don’t know if there are any more conditions I need for the calculation, because in this way, some of the protection point cannot be applied. So I would like to know how I should select the RT1 and RT2 for the temperature protection function?
Best regards,
Randy