This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25148: Dual phase schematic review request

Part Number: LM25148
Other Parts Discussed in Thread: LM5148, LM25143

Tool/software:

Hi,

I am currently designing a PSU using LM25148 dual phase to output 12V @30A using a 6S battery as power source. I need to check if I am doing anything wrong with the schematic before moving on to PCB design.
Schematic and Quick start calculator are attached below. Not sure if I filled the file correctly.

I am new in PCB design so any advice will be appreciated.

Thank you.

3618.PSU.pdf

LM5148_LM25148_quickstart_calculator_A3.xlsm