Other Parts Discussed in Thread: TPS22990
Tool/software:
Hi Teams.
I used the architecture of TPS62870 + TPS22990.
And have some question shown as below.
Q1. For TPS62870 if hold EN (active low), is i2c could be control? until I set the voltage which I need then release EN pin.
Q2. When the voltage setting is by the i2c to control, due to the output voltage has many variations, the output inductor has been fix. Will it have any impact?
Q3. For TPS62870 which soft-start ramp just 500us / 1ms/ 2ms/ 4ms. thus I use the load switch TPS22990 for more ramp time control.
but as section 9.3.2 mentioned. the output voltage seems be 5V, 3.3V, 1.8V, 1.05V and 0.6V. as my architecture the TPS22990's input will be TPS62870 output.
If i'd like to set the voltage 1.2V & 1.8V for the TPS22990 and the rise time would like to be 10ms and 100ms. how to set the Ct?
Thanks.
Best Regards
Lara