This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25302: BQ25302: Is Q1 (input FET from VBUS to PMID) disabled when /EN is high (disabled)?

Part Number: BQ25302


Tool/software:

Hi there,

The BQ25302 is disabled when /EN is pulled high. This disables the charger functionality and can be used to reset a fault condition.

Is Q1 (input FET from VBUS to PMID) also disabled when /EN is high?

The application is where a PFET (Q4) is used  for an external Power Path and the microcontroller is supplied from PMID (VSYS). If the microcontroller pulls the /EN pin high and Q1 switches off then it will be supplied via the body diode of Q1 with an increased voltage drop which is not ideal. I couldn't find any specs in the datasheet regarding the body diodes of the FETs.

Thanks in advance,

Pieter