Tool/software:
Hello, I have an application where I will need to connect either LEDs or low power RGB laser diodes to the LP5861T. For the laser diode case there is no problem with red or blue since they both need well below +5V to operate. However most green laser diodes require more like 6 to 7 volts to operate. Would I be able to power the green laser diode channel with a +7V rail voltage and then put a resistor to GND on the drive channel to ensure that even when off there will be a small amount of current that forward biases the Green laser diode so that the voltage on the output drive channel never goes above +5.5V. I could also use a Zenor diode for extra protection.
All it takes is a few milliamps on the green laser diode to create a 3 volt drop across the diode so the voltage at the output drive pin would never be higher than 7 - 3 = 4Volts. I realize this will cause the built in LED open/short function to maybe not work properly but that is not a problem for my application. I know there are other ICs I could use but the bit depth on the Global / Color Bank / and Individual Current control are features I need to accurately control the output current. Will this be OK to do?