This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65313-Q1: Automotive PMIC IC Recommendation

Part Number: TPS65313-Q1


Tool/software:

Hi,

We are developing a Level 3 autonomous tractor and are currently working on the power supply component identification for a 12V vehicle battery-powered system to drive a PMSM motor for the autosteer sub-module.

In our power supply design, we have identified the PMIC TPS65313-Q1 for the autosteer ECU board. Could you please advise if this component is suitable for our design?

Our power supply design specifications are as follows:

  • Input: 12V vehicle battery (Range: 4.5V to 36V)
  • Output 1: 3.3V, 2.5A (Buck)
  • Output 2: 5V, 600mA (Boost converter from Output 1 - 3.3V. Designed to withstand cold crank where battery voltage may drop to 4.5V)
  • Output 3: 1.8V, 1A (Buck/LDO from Output 1 - 3.3V)

Could you kindly suggest a suitable PMIC for our design?

Regards,
Jacob