This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22968: Query on impact of applying 3.3V at VOUT1

Part Number: TPS22968

Tool/software:

Hello ,

We are using  switch --> TPS22968QDMGRQ1 in our design to switch 3.3V to  peripherals on the board (RAM, FLASH etc) .

That means our peripherals will be enabled only when microcontroller is flashed  (PS1_EN = HIGH). But during production we want to program the FLASH memory for that we have to supply the 3.3V power  to it. We provided test points at the TPS outputs. Question is can we apply 3.3V to the outputs of TPS directly in production ? whether it will impact the TPS device ? or any chances of reverse voltage flow  (But datasheet i dint see body diode) .  Kindly let me know your feedback at the earliest

Regards,

Shyamasundar.