Tool/software:
Hi,
I recently designed a battery management board making use of the BQ77PL900 as an AFE & battery management chip. However, I am having some issues with the FETs as well as temperature and power consumption.
The schematic and BOM are attached below. The issues are as follows:
- PMS is 27.42 volts, PACK is 27.97 volts (at 30v to BAT+)
- D5 forward voltage is 0.02v
- Voltage drop over R14 is nothing, R12 same thing
- R14 voltage is 29.37, R12 voltage is 27.97, PACK is 27.98
- Both FET gates are at 29.97 and 27.97 volts respectively.
- The chip is getting hot to the touch with no load on the battery and no code being run on the host microcontroller.
- The FETs do not seem to react to any sort of voltage condition, or manual control through I2C. I am able to communicate with the BQ77PL900 through I2C and alter the data in registers, but the FETs do not react to these changes.
I have been struggling with this issue for a while now, and I would love some guidance in the right direction to solving this issue.