This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS922055DRRREVM: output switching behaviour vs. measured intensity

Part Number: TPS922055DRRREVM
Other Parts Discussed in Thread: TPS922055,

Tool/software:

Hello,

we want to use the TPS922055 for the illumination of a camera. Currently we have a testsetup with the eval kit TPS922055DRRREVM. For this case we need a high resolution from the LED-driver as well as a short exposure time  of 100 μs. The exposure time is triggered by an external trigger (in the diagram shown as clock). Another problem is the standby time, because the LED-driver only gets triggered every 300 ms. We would like to achieve a very smooth low ouput from our LED (yellow) over the full duration of the trigger-impulse.

We would like to use the flexible mode but didn’t get it to work yet with the irregular pulses. How can we achieve this while still remaining a fast activation and deactivation speed?

Pink: shows the ADim-Channel that’s always on => Is directly connected to the TPS922055

Purple / Blue: shows the PWM-Signal while triggered. Between each trigger-impulse it is set to send a 150 ns long pulse every 50 ms to not activate the standby  => Is directly connected to the TPS922055

Yellow: the signal comes from a Photodiode that shows the brightness of the LED

Green: it is labeled as clock and represents the wanted trigger behavior

Thanks a lot

Lukas Bunk and Markus Weber