Part Number: UCC21530-Q1
Tool/software:
hello Ti experts,
i met three problems when using driver chip UCC21530-Q1 and need your professional advice, as follows,
1. according to the content of chapter 8.3.4 from datasheet, the driver output has an internal gate voltage booster function using an internal pull-up NMOS. My question is when to open pull-up NMOS and when to close the pull-up NMOS?
2. how to check if it's suitable to open the pull-up NMOS for i think drivers chip cannot measure the mos's gate voltage in order to know miller voltage drop period.
3. There has an abnormal phenomenon: during dual pulse test(lower mos as target device and upper mos is short-circuited with inductor) the upper mos's gate voltage will drop below 0V voltage rather than 0V when increasing DC link high voltage.
our driver design is the same as example circuit in datasheet, you can refer to the figure below,

Thank you~