Other Parts Discussed in Thread: LM5045
Tool/software:
We need to design a series of isolated converters with "12V" (down to 9V) or "24V" (up to 28.8V) input and 10A, 24V output. Which would be the most efficent TI solution? Cost and size are secondary concerns, I am looking for a peak efficiency >95% and a robust, long lasting solution even with elevated temperatures (40°C ambient and limited airflow).
Are the LM5035 or the LM5045 suitable or would there be a more efficient way?