This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5012-Q1: Looking for alternative for dual output

Part Number: LM5012-Q1
Other Parts Discussed in Thread: LM5012, LM5137, LM5013

Tool/software:

I am using LM5012 with 5V output in my design currently.

I am looking for a buck converter IC with Dual output with output requirement as

1. 5V, 2A

2. 12V 2A

Maximum input voltage should be 80V to 100V

I am open for integrated switch or external switch type

Can you please suggest suitable options?