This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR54410: Absolute Maximum Ratings

Part Number: LMR54410


Tool/software:

Hi team,

I measured the oscillation waveform of the SW pin at 17.6V input, and found that it exceeded the maximum rated value of -0.3V at the falling edge by 10ns and -4.9V at the peak.
Is there any problem with exceeding the absolute maximum rating if it is instantaneous?

Best Regards,
Ryu.