This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR36006-Q1: Is 12V output from LMR36006 possible

Part Number: LMR36006-Q1
Other Parts Discussed in Thread: LMR51606-Q1, LMR36503-Q1, LMR36006

Tool/software:

Hello team,

Good day!

We are planning to use LMR36006-Q1 in one of our Zone ECU application.

Requirement

Vin = 6V to 60V 

Nominal Vin = 24V

Vout  = 12V

Iout max = 0.15A

For the above requirement, we are planning to use LMR36006-Q1 since the Vout max mentioned in site is 57V but in datasheet I'm seeing discrepancy since Vout max is not mentioned. Please confirm whether this part is best fit for my application.

Also we are considering LMR51606-Q1 as a alternative option, Is this part also suitable for the application?

When I was checking in WEB BENCH none of the above parts been suggested. Why?

Thank you!