This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS546A24AEVM-1PH: Regulation of current/voltage

Part Number: TPS546A24AEVM-1PH

Tool/software:

Hey Team,
the part TPS54A24A has an output voltage range from 0.25V to 5.5V. In the data sheet of the evaluation board TPS54A24AEVM-1PH with the named part it says the output voltage is regulated on a fixed output voltage of 1.2V and the current is variabel from 0 - 10 A (table 2.1). On page 5 in the figure 3.1 the Output Voltage has a range of 0.25V to 5.5V at 10A. So now the quarion is it possible to regulate the output voltage and the output current with the evalutaion board at the same time or is the output voltage fixed at 1.2V.

Thank you very much!

Best regards
Tobi Kussinger.

  • Hi Tobi

    The EVM can regulate single Vout with full output current range.

    The EVM application is set to 1.2V Vout which can out put any current from 0-10A and

    if you need a different regulating voltage you can make appropriate changes to EVM as suggested in EVM user guide and IC datasheet and operate with full output current range

    Thank you

    Savith